AIN#.DEADBAND
Description
AIN#.DEADBAND sets the deadband of the analog input signal.
When AIN#.DEADBANDMODE is set to 0, and the value of the analog input is less than the absolute value of AIN#.DEADBAND, the analog command will be 0. When the analog input is greater or equal to the absolute value of AIN#.DEADBAND, then the analog command will be generated using the scaling specified.
When AIN#.DEADBANDMODE is set to 1, the analog command is 0 if the input is less than the absolute value of the deadband. When the input is greater than the absolute value of the deadband, the output is equal to (Input - Deadband) * Scaling.
Below are illustrations of this behavior.
Examples
Context
For more information see Analog Input.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type | Read/Write |
Units | V |
Range | 0 to 12.5 |
Default Value | 0 |
Data Type | Float |
See Also | |
Stored in Non-Volatile Memory | Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
|
---|---|---|---|---|---|---|---|
AIN1.DEADBAND |
3780h |
04h |
Signed16 |
- |
1000:1 |
Read/Write |
No |
AIN2.DEADBAND |
3781h |
04h |
Signed16 |
- |
1000:1 |
Read/Write |
No |
Name |
ID |
Hex |
Data Type |
Access |
Units |
---|---|---|---|---|---|
AIN1.DEADBAND |
23150 |
5A6E |
Signed16 |
Read/Write |
- |
AIN2.DEADBAND |
23151 |
5A6F |
Signed16 |
Read/Write |
- |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
AIN1.DEADBAND |
23150 |
Float |
Read/Write |
- |
AIN2.DEADBAND |
23151 |
Float |
Read/Write |
- |